text.skipToContent text.skipToNavigation
Leading standard

Norms and standards

The products you purchase on Fabory.com meet the strictest standards, including DIN and ISO. These are leading organisations in the development of technical standards. DIN focuses on national German standards, while ISO handles globally recognised standards. The guidelines promote uniformity, safety, and quality across various industries. We will explain the two standards in more detail below:

DIN (Deutsches Institut für Normung):

Many people are familiar with the term DIN, but what does this standard represent? DIN stands for Deutsches Institut für Normung, a leading German standard organisation responsible for defining DIN standards for fastening materials and industrial products. Much of our materials adhere to DIN standards, ensuring quality and consistency.

din934

DIN 934

Hatlap anya

Termék megtekintése

Zeskantbout

DIN 931

Hatlap anya

Termék megtekintése

DIN 933

DIN 933

Hatlap anya

Termék megtekintése

DIN 7991

DIN 7991

Hatlap anya

Termék megtekintése

History

DIN was established in 1917 as the 'Normenausschuss der Deutschen Industrie' (NADI). The organisation aimed to set standards for the German industry but quickly became a key player on the international stage. As a result, the name was changed in 1926 to 'Deutscher Normenausschuss' (DNA), highlighting the broader application of standards beyond the industry.

Structure and collaboration

After World War II, DIN was reestablished and renamed 'Deutsches Institut für Normung.' The focus was now on rebuilding the German economy and promoting international cooperation. During the 1950s and 1960s, DIN played a crucial role in founding the International Organisation for Standardisation (ISO) and the European Committee for Standardization (CEN).

Quality and reliability

Today, DIN is one of the world's leading standard institutes and sets standards for nearly every conceivable product and process. DIN standards are synonymous with quality and reliability. With over 34,000 standards in its portfolio, DIN contributes to harmonising technical standards worldwide and promotes innovation, safety, and sustainability in various sectors. We are proud that most of our products are certified according to DIN standards.

ISO and DIN fastening standards

ISO (International Organisation for Standardisation):

ISO standards are globally recognised as the benchmark for quality and safety. Our products meet various ISO standards, such as ISO 9001 for quality management and ISO 14001 for environmental management.

History

ISO was established in 1947 and has grown to become one of the most influential standardisation institutes worldwide. It originated from the International Federation of the National Standardising Associations (ISA), active from 1926 to 1942 but ceased during World War II. Following the war, international technicians realised the need for a new and widely supported institute for global standardisation, leading to the establishment of ISO.

Equality

ISO is derived from the Greek word 'isos,' meaning 'equal.' It symbolises universal equality and standardisation, regardless of the language in which the abbreviation is pronounced. Quality, environment, and information Since 1945, ISO has developed thousands of international standards that are used worldwide in various industries. Notable standards include ISO 9001 (quality management), ISO 14001 (environmental management), and ISO 27001 (information security).

Operating uniformly

The International Organization for Standardisation (ISO) is a worldwide platform that harmonises technical standards. It provides a common language and basis for product quality, safety, and sustainability. ISO standards promote trade, innovation, and consumer protection while assisting organisations in different countries to operate uniformly. Fabory is proud to make a significant contribution to this way of working.

ISO10642

ISO 10642

Hatlap anya

Termék megtekintése

ISO4014

ISO 4014

Hatlap anya

Termék megtekintése

ISO4035

ISO 4035

Hatlap anya

Termék megtekintése

ISO4032

DIN 934 A2

Piuliță hexagonală

Vezi produsul

EN (European Norm)

Standardele europene, cunoscute și sub denumirea de EN, sunt standarde tehnice dezvoltate în Europa pentru a asigura că produsele și procesele îndeplinesc cerințe uniforme de calitate. Comitetul European de Standardizare (CEN) elaborează aceste standarde în colaborare cu diverse organizații europene. Ele stimulează comerțul, asigură condiții de lucru sigure și fac produsele mai fiabile în sectoare precum construcții, automotive și aerospațial. În domeniul construcțiilor, de exemplu, sunt utilizate șuruburi structurale conforme cu standardele EN 15048 sau EN 14399.

Istorie

Standardele EN au fost create pentru a uniformiza calitatea și specificațiile tehnice în Europa. De la înființarea sa în 1961, CEN a jucat un rol esențial în dezvoltarea unor standarde comune care să înlocuiască reglementările naționale contradictorii. Această armonizare facilitează comerțul internațional și garantează un nivel constant de calitate și siguranță.

Structură și colaborare

Standardele sunt dezvoltate de experți tehnici din peste 30 de țări. Peste 60.000 de profesioniști contribuie cu expertiză pentru a se asigura că standardele reflectă cele mai noi evoluții și tehnologii industriale. Procesul se bazează pe colaborare, transparență și consens, cu implicarea industriei, a guvernelor și a organizațiilor sociale. Această colaborare asigură că standardele EN sunt nu doar tehnic solide, ci și larg acceptate de industrie și autorități, ceea ce crește aplicabilitatea lor în diverse sectoare.

Calitate și fiabilitate

Elementele de fixare conforme standardelor EN sunt supuse unor teste riguroase privind proprietățile lor, cum ar fi rezistența mecanică, rezistența la coroziune și durabilitatea. Acest lucru garantează că producătorii livrează produse fiabile pentru aplicații critice. De exemplu, elementele de fixare conforme EN 1090 sunt testate pentru capacitatea lor de a rezista la sarcini mecanice, un aspect crucial pentru integritatea structurală în construcțiile metalice. Respectarea acestor standarde ajută, de asemenea, la îndeplinirea reglementărilor UE, facilitând accesul pe piață și consolidând încrederea dintre furnizori și clienți.

Pe scurt, standardele EN sunt esențiale pentru garantarea calității, siguranței și oportunităților de comerț internațional. Ele permit companiilor din orice țară să se bazeze pe produse care îndeplinesc constant standarde înalte.

Leadingpage HV

EN 14399

Piuliță hexagonală

Vezi produsul

EN 15048

EN 15048

Piuliță hexagonală

Vezi produsul

EN 16983

EN 16983

Piuliță hexagonală

Vezi produsul

EN 1664

EN 1664

Piuliță hexagonală

Vezi produsul

Experți în elemente de fixare

Cu cunoștințe tehnice, calcule și teste, asigurăm proiectarea și aplicarea corectă a elementelor de fixare specifice. Gama noastră de 120.000 de articole, în orice design, dimensiune și material, necesită o gestionare eficientă a stocurilor pe care te poți baza. Aplicația RFID este una dintre soluțiile inteligente oferite de Fabory Logic. Fiecare soluție oferă suport valoros pentru gestionarea stocurilor companiei tale. Astfel, se creează liniște, iar angajații se pot concentra pe sarcinile lor principale.

Gama de produse

Fabory este alegerea potrivită pentru toate nevoile dvs. de fixare. Portofoliul nostru de produse conține o gamă largă de elemente de fixare standard și soluții de fixare specifice pentru diverse aplicații precum si C-parts.

Fabory Logic

Fabory Logic va pune la dispozitie o gama completa de servicii lde gestionare a stocurilor printre care RFID, Optical-Eye, Cântare și Merchandiser

Inginerie si controlul calitatii

Fabory este construit pe calitate și fiabilitate. Managementul calității este în centrul operațiunii noastre. Inginerii noștri sunt disponibili pentru a vă sprijini în asigurarea alegerii corecte a elementelor de fixare.

Ne zárja be ezt az oldalt. Ez az üzenet eltűnik, amikor az oldal teljesen betöltődik.